2 Replies Latest reply: Jan 19, 2011 8:51 AM by rele RSS

Few question Back-UPS ES 550G --self-test--Overload Shutdown - Funny result

rele Member
Currently Being Moderated
I have Back-UPS ES 550G
Firmware revision: 870.O2.I
Software version: PowerChute Personal Edition 2.0

It shows:
Result of last manual self-test is: Unsupported
And tehnical data:
Last manual self test date: Unsupported
*1.*what is this meaning?
-----
*2.*Do this model have Overload Shutdown?
[http://www.apcmedia.com/salestools/ASTE-6Z7V9M_R0_EN.pdf]

Says that there is Overload Shutdown, but who knows if it is automatic?

-----
*3*.Funny result, is this possible, did i miss something?

I get digital multimeter total load: 0.78A
0.78A x 230V = *183.3 VA*

And

This is what i get UPS Selector
-( Extra Power for future expansion value 0%)

-(AMD Athlon 64 2800+ is missing on list

i used AMD Athlon 64 2600+ )
Result:
APC Smart-UPS 1000VA LCD 230V
% of Max Capacity Used: 54 % = ( *540 VA* )

More Like This

  • Retrieving data ...