3 Replies Latest reply: Jan 11, 2010 12:33 PM by Techie RSS

Continuous beep, no power loss, green light

digitalpackrat Member
Currently Being Moderated
My 350 is about five years old, I think. I've never replaced the battery, the light has always been green on it during normal function. Recently, every once in a while, I will suddenly get a long, continuous beep...much as it does every time I lose power, since the battery is in need of replacement.

At the times I am asking about, however, the power is still on...so I'm assuming the amount of power in the battery doesn't matter, right? I honestly don't know if it would randomly alert me, especially since the light remains green when this happens. The only things plugged into it are my computer, monitor, and speakers...same things as always, so it shouldn't be overloading. I suffer no interruption in power to my computer when this happens. Just this annoying tone that will go away if I press the button on the battery backup itself off, then on again.

More Like This

  • Retrieving data ...

Legend

  • Correct Answers - 8 points
  • Helpful Answers - 4 points