1 Reply Latest reply: Nov 25, 2009 8:51 AM by TaSpEc RSS

netbotz rack monitor 200 sends email - but temperature not shown

captainjamestkirk Member
Currently Being Moderated
just setup our netbotz rock monitor 200.

it sends an email when over a certain threshold (82 degrees right now), but doesnt include the temperature.
just a "high temperature threshold violation" is in the email, not the temperature.

how do I get it to email me the temperature each time?

More Like This

  • Retrieving data ...

Legend

  • Correct Answers - 8 points
  • Helpful Answers - 4 points