3 Replies Latest reply: May 18, 2012 8:37 AM by Jon P. RSS

Back-UPS 550 and PCPE 3.0.2 - no self-test and no battery date

scistan Member
Currently Being Moderated
I have many Back-UPS 550 running PowerChute Personal Edition 2.0 on Windows XP workstations. With PowerChute I can run a self-test, I can see the battery replacement date and I can update the battery replacement date. I don't see those features in version 3, which is required for Windows 7 or when I upgrade to v3 on XP. Those seem like pretty valuable features. How they been removed in v3? Is something wrong with my install? Is this specific to this model of UPS?

More Like This

  • Retrieving data ...

Legend

  • Correct Answers - 8 points
  • Helpful Answers - 4 points