Loading ...

galaxy 5500

Discussion in Data Center & Facility 3 Phase UPS started by saeid , 1/16/2018 6:28 AM
Login to follow, share, and participate in this space.
Not a member?Join now
  • saeid1987
    saeid
    New Member New Member
    saeid 1/16/2018 6:28 AM

    Hello
    I have a problem starting ups
    It has errors

  • wpasquil
    Bill
    =S= Representative
    Bill 1/17/2018 2:50 PM (in response to saeid)

    Hi,

    I asked the 3 phase support team in in the U.S. and they recommend you contact local support for assistance. The error indicates you will need a technician dispatched to troubleshoot.

    Local support contact information will be found at this link http://www.apc.com/ae/en/support/contact-us/index.jsp

  • dorado
    jesus
    Novice Novice
    jesus 3/1/2018 3:17 PM (in response to Bill)
    buenos dias la falla que comentas se debe por lo general a un mal proceso de encendido el cual provoca una averia en el FU7
    verifica el estado del mismo y revisa que todas las tarjeta esten con los voltajes correctos.
    el encendido debe ser realizado con el Tunner para evitar que la rampa vuelva a averiar el fusible una ves se aya conluido la carga este funciona normalmente.
  • dorado
    jesus
    Novice Novice
    jesus 3/1/2018 3:17 PM (in response to jesus) good morning the fault you say is usually due to a bad ignition process which causes a breakdown in the FU7 check the status of the same and check that all the cards are with the correct voltages. the ignition must be carried out with the Tunner to prevent the ramp from damaging the fuse once the load is working normally.
  • daniyal
    daniyal
    Novice Novice
    daniyal 3/10/2018 7:32 AM (in response to saeid)

    salam

    man fekr mikonam shoma irani hastid.

    fault pfc shoma ehtemalan b khatere in bode k control position bar roy swich cabinet battery nasb nashode bode va ghabl az run shodan sharjer swich battery ra vasl kardeid va dar hal hazer fuse mohafeze pfc va ya borde charger asib dide

    dar morede moshkele dovom ham bayad az tarighe narm afzar ups tuner disabel beshe va moshkele khasi nist.

  • Page 1 of 1 (5 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692