Loading ...
home » spaces » Data Center & Facility 3 Phase UPS » discussion » General » Smart UPS - SUVTP10kH2B2S UPS: In bypass in response to an internal hardware fault

Smart UPS - SUVTP10kH2B2S UPS: In bypass in response to an internal hardware fault

Discussion in Data Center & Facility 3 Phase UPS started by Mohammed , 5/26/2017 5:02 AM
Login  to follow, share, and participate in this space.
Not a member?Join now
  • arifm
    Mohammed
    New Member
    New Member
    Mohammed 5/26/2017 5:02 AM

    Hello All,

    We have 2 UPS in parallel configuration on a location. Recently both the UPS just shutdown itself as well as the load, however just before the shutdown following alerts were received from UPS. we had 2 instances of UPS complete shutdown within 36 hours.

    Device UPS: The external Switch Gear Q004 has opened.
    Device UPS: The output power is turned off.
    Device UPS: In bypass in response to an internal hardware fault.
    Device UPS: Return from bypass, internal hardware fault no longer present.
    Device UPS: In bypass in response to an internal hardware fault.

    On First Instance found as below;

    UPS was totally Shutdown & No Display.

    The MCB supplying mains input power to UPS were tripped.

    On Second Instance

    UPS was totally Shutdown & No Display.

    We would like to have your expertise for the below queries;

    • What are the reason for UPS to generate an internal hardware fault.
    • Why did the UPS Shutdown completely.
    • What had caused the MCB to trip.
    • Though the battery were still within the UPS, why didn’t UPS go on battery power rather than shutting down.

  • wpasquil
    Bill
    =S= Representative
    Bill 5/26/2017 4:24 PM (in response to Mohammed)

    Hi,

    You should contact local support for assistance. They will require logs and help you troubleshoot the issue. You will find local support contact information at this link

    http://www.apc.com/us/en/support/contact-us/index.jsp

  • Page 1 of 1 (2 items)
Choose your language:  English  
powered by Communifire
Version 5.0.5741.40378