Loading ...
Home » Spaces » UPS Management Devices & PowerChute Software » discussion » General » Powerchute BE can't find SMT750 via USB.

Powerchute BE can't find SMT750 via USB.

Discussion in UPS Management Devices & PowerChute Software started by Mr. , 21 days ago
Login to follow, share, and participate in this space.
Not a member?Join now
  • MrPerfect
    Mr.
    Novice Novice
    Mr. 21 days ago

    Hello all,

    I'm attempting to install PowerChute BE on a Windows 10 Pro workstation(version 1703, AKA Creators Update) with a SMT750 hooked up to it via USB cable, but PowerChute simply can't find the UPS. Windows does see the UPS, and lists it in Device Manager as both an "APC UPS" in the Batteries section and as "American Power Conversion USB UPS" in the Human Interface Devices section.

    Device Manager

    The APC USBTerm.exe program that has been linked to on the forums here also sees the UPS. It successfully pulls the model, firmware versions and serial number for the UPS.

    USBTerm

    I've tried both PowerChute BE v9.1.1 and v9.2.1.

    Any ideas? frown

    Thanks,

    MP

  • wpasquil
    Bill
    =S= Representative
    Bill 21 days ago (in response to Mr.)

    Hi,

    Sorry for the inconvenience. Is PowerChute failing to install or once installed is it reporting that it cannot communicate with the UPS?

  • MrPerfect
    Mr.
    Novice Novice
    Mr. 20 days ago (in response to Bill)

    Hi, thanks for helping.

    The Powerchute Agent does install, it just doesn't find the UPS during or after setup. The first screen in the setup wizard says it can't find the UPS automatically, and prompts me for the connection type.

    Manual selection

    I just leave it at DB9 and hit OK. A little later in the setup wizard I get the option to define what the UPS is, so I fill in Smart-UPS and USB.

    Manual definition

    Installation completes, but when logging into the agent it can't establish a connection.

    Not established

    Should I be using different settings?

    Thanks,

    MP

  • wpasquil
    Bill
    =S= Representative
      This discussion is marked as answered
    Bill 20 days ago (in response to Mr.)

    Hi,

    Select RJ45 and then proceed with the installation. Selecting RJ45 tells PowerChute that the UPS is a SMT. 

  • MrPerfect
    Mr.
    Novice Novice
    Mr. 20 days ago (in response to Bill)

    Oh, wow. You're absolutely right, that's fixed it. Thanks Bill! smile

  • Page 1 of 1 (5 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692