Loading ...
Home » Spaces » UPS Management Devices & PowerChute Software » discussion » General » Configuring syslog through CLI

Configuring syslog through CLI

Discussion in UPS Management Devices & PowerChute Software started by J , 12/23/2015 3:08 PM
Login to follow, share, and participate in this space.
Not a member?Join now
  • ezbrezzy
    J
    New Member New Member
    J 12/23/2015 3:08 PM

    Is there no option on AOS 6.2.1 to configure syslog settings through CLI with the NMC type AP9631? 

  • ipicKedawinna
    Angela
    =S= Representative
    Angela 12/23/2015 3:10 PM (in response to J)

    Hello,

    I don't see it. And I also checked v6.4.0 which will be released in the next week or so. I only see it available to configure via the web UI or config.ini configuration file as of today. I will log an enhancement request to see if we can add it in a future release.

  • ezbrezzy
    J
    New Member New Member
    J 12/23/2015 3:11 PM (in response to Angela)

    Thanks! 

  • jamess
    James
    Novice Novice
    James 11/10/2016 4:29 PM (in response to Angela)

    I have over 250 APC's I manage. being forced to use the web interface is rough.

    I script everything in VBScript/Secure CRT.

    any recommendations for me?

  • ipicKedawinna
    Angela
    =S= Representative
    Angela 11/10/2016 6:59 PM (in response to James)

    Perhaps using the config.ini file offered with the Network Management Card platform? Below is an exerpt from it. You can configure Syslog settings among many others in this file and then use FTP (we offer a free utility to do this - called INI Utility) or SCP or our StruxureWare Data Center Expert appliance to cascade this file and the same settings across multiple units.

    [NetworkSYSLOG]
    Syslog=enabled
    Facility=User
    Server1=0.0.0.0
    Server2=0.0.0.0
    Server3=0.0.0.0
    Server4=0.0.0.0
    Port1=514
    Port2=514
    Port3=514
    Port4=514
    Protocol1=0
    Protocol2=0
    Protocol3=0
    Protocol4=0
    Language1=enUs
    Language2=enUs
    Language3=enUs
    Language4=enUs
    SyslogMapCritical=Info
    SyslogMapWarning=Warning
    SyslogMapInformational=Info

  • evbstv
    Eduardo
    New Member New Member
    Eduardo 3/13/2018 2:31 PM (in response to Angela)

    Did anyone ever wonder why Critical & Informational syslogs map similarly to Info?

    SyslogMapCritical=Info
    SyslogMapWarning=Warning
    SyslogMapInformational=Info
  • Page 1 of 1 (6 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692