Loading ...
Home » Spaces » Racks, Rack Accessories, & Cooling » discussion » General » Bug in Firmware , Daylight Saving (DST) options , PDU AP7920

Bug in Firmware , Daylight Saving (DST) options , PDU AP7920

Discussion in Racks, Rack Accessories, & Cooling started by Vincent , 3/31/2016 1:59 PM
Login to follow, share, and participate in this space.
Not a member?Join now
  • vsnijder
    Vincent
    Novice Novice
    Vincent 3/31/2016 1:59 PM

    Hello ,

    I hope this is the right place to report a bug?

    It seems there is a bug regarding the Daylight Saving Options (DST) in the firmware for our AP7920 's.

    Latest firmware is installed :

    rpdu Version: v3.7.4

    aos Version: v3.9.0

    Here in Europe we use : last Sunday March / last Sunday October

    To start with , the settings are even conflicting/contradicting in itself (?!). You can select "fourth/last" or "fifth/last".

    Screenshot of DST settings

    Now... the fourth can never be the last, if there is a fifth that given year ... 

    And "fifth' can not be a valid option, as this does not occur every year.

    ("Chicken or the Egg" , anyone?)

    So the valid options to match rule-sets , SHOULD simply be : first/second/third/fourth/last

    Secondly, selecting "fifth/last" (as it should be in my case?), does not work.

    The time then changes on the second Sunday in March (?!) , as I have noticed this month.

    Selecting fourth/last seems to work (on the fourth Sunday), but is not correct for our DST- schedule (last Sunday).

    In years when there is a fifth Sunday, it will also switch on the fourth.

  • fabsainte
    fab
    Novice Novice
    fab 4/1/2016 10:40 AM (in response to Vincent)

    +1

    same issue with AP7721 and latest firmware v3.9.0, trying to configure France daily saving times...

  • ipicKedawinna
    Angela
    =S= Representative
    Angela 4/1/2016 5:12 PM (in response to Vincent)

    Hi - I'll have the local support in EMEA region double check the settings and confirm what the bug affects and then we'll go ahead and log it. I'll let you know if we have further questions on this, else, we'll log a bug about it with what you provided.

    Thanks for providing the details of the specifics.

  • vsnijder
    Vincent
    Novice Novice
    Vincent 4/1/2016 6:23 PM (in response to Angela)

    Great !

    I also just happened to find this post, dating back to 2010 :

    http://forums.apc.com/spaces/7/ups-management-devices-powerchute-software/forums/general/6646/dst-doesn-t-work-correctly-with-german-rules

    But it is regarding  a Network Management Card, I believe.

    And the thread stops without a (public) solution.

  • ipicKedawinna
    Angela
    =S= Representative
    Angela 4/1/2016 6:28 PM (in response to Vincent)

    Yeah, that one was on our second generation Network Management Card 2 (NMC2). AP7920 uses the older generation NMC1. We can never seem to get DST correct apparently wink

    I'll report back next week when I presume I'll log the bug after EMEA team double checks DST for EMEA regions (I hope).

  • BlueSky
    Joe
    Apprentice Apprentice
    Joe 4/1/2016 8:37 PM (in response to Angela)

    My apologies for the flippant remark, but I recommend you focus all your efforts on getting the governments of the world to scrap DST altogether.  cool  I really dislike having to change all the clocks and watches in my house!

  • vsnijder
    Vincent
    Novice Novice
    Vincent 8/18/2016 4:38 PM (in response to Angela)

    **Bump**

    Any update on this??

  • TomT
    Tom
    New Member New Member
    Tom 3/13/2017 8:32 PM (in response to Vincent)

    This was reported a year ago and the bug still exists (even though there has been a subsequent firmware update to v3.9.2)

    Is there ever going to be a fix for this? We have scheduled power changes and this really messes our systems up.

  • Page 1 of 1 (8 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692