Loading ...
home » spaces » Smart-UPS & Symmetra LX / RM » discussion » General » smart ups 1400 whistles

smart ups 1400 whistles

Discussion in Smart-UPS & Symmetra LX / RM started by aldo , 8/3/2007 8:33 PM
Login  to follow, share, and participate in this space.
Not a member?Join now
  • sugar
    New Member
    New Member
    aldo 8/3/2007 8:33 PM

    Hi, why the smart ups 1400 one day it is just whistling?
    I made a self test and it is silent again...
    is that normal? or is it a warning of a malfuncioning?

    Thanks in advance


  • Syn
    Tim 8/3/2007 8:50 PM (in response to aldo)

    could you be a bit more specific about the noise? Did anything happen before it started (storms, surges)? What kind of temps do you see around the unit?
    Any other alarms or indicators?


  • sugar
    New Member
    New Member
    aldo 8/3/2007 10:47 PM (in response to Tim)

    no storms, no rains, just lot of humidity and hot days...
    the front box doesnt show any warning, only a whistle like when it does a self test...

  • KVM4Life
    =S= Representative
    Joshua 8/4/2007 2:10 AM (in response to aldo)


    Do you remember what lights were lit and could you describe what the sound was like. Was it constant, intermittent, more like a tone? Are you saying that simply running the self test cleared the sound or did this sound only occur during the time you heard the whistling sound? What do you have plugged into the unit? Are you using Powerchute with the UPS? If so, did powerchute log any events around the time of the whistling sound?

  • KVAr
    KVar 8/4/2007 8:26 PM (in response to aldo)

    There should be one green light lit on the front. There should be no beeping, although you may hear the fan.

  • InRowRCena
    Oscar 8/9/2007 6:41 PM (in response to aldo)

    Sometimes the UPS will emmit a beep when there's a quick fluctuation of power. It attempts to go on battery but since utility power is restored right away, all you'll hear is a beep, and you will not see the on battery LED.

  • Page 1 of 1 (6 items)
Choose your language:  English  
powered by Communifire
Version 5.0.5741.40378