Loading ...
Home » Spaces » Smart-UPS & Symmetra LX / RM » discussion » General » 2200 VA - no power

2200 VA - no power

Discussion in Smart-UPS & Symmetra LX / RM started by Lex , 3/6/2018 4:03 PM
Login to follow, share, and participate in this space.
Not a member?Join now
  • UncleRick
    Lex
    Novice Novice
    Lex 3/6/2018 4:03 PM

    Have a small issue with the 2200 VA we have. Moved it from one rack to another (battery packs removed while moving) and now the unit won't power on at all.

    Batteries removed while moving the unit, reconnected after. Not powering on at all. When input power is connected, the "sensitivity" indicator comes on, there a click and all the light on the front panel flash once. And then nothing - no pass-through power, no self-test, no power at all except the "sensitivity" light at the back.

    Any ideas?

  • liamg
    Liam
    =S= Representative
    Liam 3/6/2018 9:14 PM (in response to Lex)

    It could be faulty batteries. Do you have a known good set of batteries you could try or a voltmeter to test the voltage of the batteries you are attempting to use?

  • UncleRick
    Lex
    Novice Novice
    Lex 3/7/2018 12:06 PM (in response to Liam)

    No spare batteries. I'll test the batteries with the voltmeter.

    Doesn't make  sense though. Working perfectly fine, disconnected for 15 minutes, and suddenly they are faulty when reconnected?

  • UncleRick
    Lex
    Novice Novice
    Lex 12 days ago (in response to Lex)

    So tested both packs with a voltmeter - DC output is 27.8V and 25.3V.

    Seems to be good enough, no?

    It's a SU2200RMI3U to be exact.

  • Page 1 of 1 (4 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692