Loading ...
Home » Spaces » Smart-UPS & Symmetra LX / RM » discussion » General » Setting up email notification is failing in Powerchute Business v9.2

Setting up email notification is failing in Powerchute Business v9.2

Discussion in Smart-UPS & Symmetra LX / RM started by Haider , 1/9/2018 7:16 PM
Login to follow, share, and participate in this space.
Not a member?Join now
  • hayder78
    Haider
    Novice Novice
    Haider 1/9/2018 7:16 PM

    I read multiple times in this forum that in version 9.2 it was possible to configure smtp servers to work with gmail. However I do not see any SSL port settings. It is still only the basic authentication which was just like in version 9.1.

    I have installed the Powerchute business edition v9.2 for Windows 8.

    Am I missing something?

  • wpasquil
    Bill
    =S= Representative
    Bill 1/9/2018 8:44 PM (in response to Haider)

    Hi,

    What is the model number of the Smart-UPS? If the model is SUA, SU, SURT, SC, then SSL port settings are not available. We will be releasing PowerChute Business Edition 9.5 soon (next 90 days) that adds SSL port settings for all Smart-UPS. 

    If the model is SMT, SMX, SRT, SURTD, SMC than the SSL port settings are available in the web interface as listed in Schneider Electric FAQ FA249593

  • hayder78
    Haider
    Novice Novice
    Haider 1/10/2018 5:25 AM (in response to Bill)

    Hi Bill,

    Model is: SMC1500i

    I did not know there is web agent. I found it and entered the email settings. Thanks

  • hayder78
    Haider
    Novice Novice
    Haider 1/10/2018 8:18 AM (in response to Bill)

    The email run well. However I have tested the shutdown and my modification to do hibernate instead of shutdown did not work. Still it is shutting down the pc.

    I am on Windows 10 pro. In the path "C:\Program Files (x86)\APC\PowerChute Business Edition\agent\bin" I renamed the hibernate.exe into shutdown.exe

    What can I do to do hibernate instead of shutdown?

  • Page 1 of 1 (4 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692