Hello All,
i am having an issue with newly installed APC smart UPS 2200VA. After installing the unit and adding load on it displayed an error on the screen Warning State: Replace battery and continuously giving me alarms. Could some one help me in fixing the issue. Have i missed something in enabling in the UPS or the battery is already defected defected.
Appears to be a SMT-2200RM unit? What are the first 4 digits of the serial numbers on the UPS and also the battery pack? I've seen "new" in-box units being sold that are over 7 years old - the batteries will not be any good.
Choose a location
discussion :
There are no forums in this space.