Loading ...
home » spaces » Smart-UPS & Symmetra LX / RM » discussion » General » Smart UPS 3000 not running off AC

Smart UPS 3000 not running off AC

Discussion in Smart-UPS & Symmetra LX / RM started by Rider , 4/6/2011 9:58 PM
Login  to follow, share, and participate in this space.
Not a member?Join now
  • PeeWee2000
    Rider
    New Member
    New Member
    Rider 4/6/2011 9:58 PM

    I recently recieved an old UPS from my mothers work and purchased new batteries for it and it seems to be working fine other than the fact that after 10 seconds it automatically switches to battery even though it is plugged in, any help would be appreciated.

  • JonPro
    Jonathan
    =S= Representative
    Jonathan 4/7/2011 4:05 PM (in response to Rider)

    Hi PeeWee,

    I would like to ask if the UPS goes back to Online mode. If not, what do you usually do to put it back to online? Is the UPS switching back and forth from Online to On Battery?

    One thing that I can recommend is for you to change the sensitivity of the UPS to a much more lower setting. Depending on the model, you can look at the back of the UPS and look for the Sensitivity button. Here is a kbase that would show you how to change the sensitivity.

    [What are the different sensitivity settings of a Smart-UPS?|http://nam-en.apc.com/app/answers/detail/a_id/62/kw/smart-ups%20sensitivity]

  • PeeWee2000
    Rider
    New Member
    New Member
    Rider 4/8/2011 12:24 AM (in response to Jonathan)

    No the AC light on the UPS blinks a couple of times then it stays off the entire time the battery light is on, wich is as long as I decide to leave the UPS on

  • ipicKedawinna
    Angela
    =S= Representative
    Angela 4/8/2011 2:01 AM (in response to Rider)

    did you try hitting the input circuit breaker next to the input power cord on the back of the UPS? maybe someone accidentally hit it or moved it?

  • PeeWee2000
    Rider
    New Member
    New Member
    Rider 4/9/2011 1:24 AM (in response to Angela)

    Thanks alot that was the problem ;D

  • ipicKedawinna
    Angela
    =S= Representative
    Angela 4/11/2011 2:12 PM (in response to Rider)

    glad to help :-)

  • Page 1 of 1 (6 items)
powered by Communifire
Version 5.0.5741.40378
Choose your language:  English