Loading ...
Home » Spaces » Smart-UPS & Symmetra LX / RM » discussion » General » It is accurate that APC will NOT cover under contract units which are 10 years old?

It is accurate that APC will NOT cover under contract units which are 10 years old?

Discussion in Smart-UPS & Symmetra LX / RM started by Boyan , 3/15/2017 5:57 PM
Login to follow, share, and participate in this space.
Not a member?Join now
  • bbiandov
    Boyan
    Apprentice Apprentice
    Boyan 3/15/2017 5:57 PM

    Hi everyone,

    It is accurate that APC will NOT cover under contract units which are 10 years old?

    I have these and I'm told they are no longer eligible for coverage under APC service contract?

    Model

    Serial #

    SURTD5000XLT

    NS0635019xxx

    SURTD5000XLTQ

    QQ1536270xxx

    SURTD5000XLT

    NS632006xxx

    SURTD5000XLT

    NS632007xxx

     

  • wpasquil
    Bill
    =S= Representative
    Bill 3/16/2017 1:40 PM (in response to Boyan)

    Hi,

    The Smart-UPS line has a maximum of 6 years of warranty. Any extended warranty must be purchased while the standard factory warranty is in effect. As an example for your units the standard warranty was 2 years and you could have purchase an additional 1 and 3 year warranty bring the units to the maximum of 6 years.  

  • bbiandov
    Boyan
    Apprentice Apprentice
    Boyan 3/16/2017 3:04 PM (in response to Bill)

    Thanks Bill,

    I'm even more confused; I was able to purchase extended contracts from APC twice -- each time for 3 years? I'm happy to share the PDF scan via PM. Has the policy changed lately? And what is the current credible and enforced extended warranty policy of APC?

    I am asking because a vendor just quoted a THIRD extension of the warranty contract for 3 more years. 

    Thanks

    ~B

  • wpasquil
    Bill
    =S= Representative
    Bill 3/16/2017 4:07 PM (in response to Boyan)

    Hi,

    The policy has not changed. It has been 6 years for Smart-UPS for the 14 years I have worked here. The issue is enforcement. People sell extended warranties even though they should not.

  • bbiandov
    Boyan
    Apprentice Apprentice
    Boyan 3/29/2017 3:09 AM (in response to Bill)

    Thanks Bill -- I don't mean to be a devil's advocate but I do need to ask:

    So if I get someone to sell me a contract -- be it a partner or reseller -- do I take it correctly that APC WILL HONOUR it?

    Thanks

    ~B

  • GoNz0
    Gareth
    Apprentice Apprentice
    Gareth 3/29/2017 7:34 AM (in response to Boyan)

    I bought one from a 3rd party that had bought it in error, it was activated without issue. Of course I had read on APC's site about warranty extension and knew the maximum was 6 years from original purchase so my 3 year warranty was extended to 6.

  • bbiandov
    Boyan
    Apprentice Apprentice
    Boyan 3/29/2017 3:25 PM (in response to Gareth)

    @gareth Excellent! That's what I needed to confirm. Thank you!

  • Page 1 of 1 (7 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692