Loading ...
Home » Spaces » Smart-UPS & Symmetra LX / RM » discussion » General » Smart UPS SU620 Not showing Internal temperature on PowerChute BE 9.1.1

Smart UPS SU620 Not showing Internal temperature on PowerChute BE 9.1.1

Discussion in Smart-UPS & Symmetra LX / RM started by Stephen , 3/14/2017 1:12 PM
Login to follow, share, and participate in this space.
Not a member?Join now
  • stedenis
    Stephen
    New Member New Member
    Stephen 3/14/2017 1:12 PM

    I am not able to see the internal temperature on my Smart UPS SU620 on PowerChute BE 9.1.1. I have to admit, I do not recall if it was present on the other versions of PCBE. It seems that this is a basic metric and should be visible.

    I just replaced the battery and performed the calibration within PCBE 9.1.1.

    Should it be viewable? If so, what should I look for to get it to sense the temperature.

  • wpasquil
    Bill
    =S= Representative
    Bill 3/14/2017 7:14 PM (in response to Stephen)

    Hi,

    I do not have a 620 available for testing but my recollection is that data point is not available. Maybe another forum member that has a 620 will help out. Some of the lower end Smart-UPS did not offer all of the same data points and the higher end ones do and that may be the case here.

  • stedenis
    Stephen
    New Member New Member
    Stephen 3/15/2017 11:49 PM (in response to Bill)

    If I had a schematic, I could figure it out myself.

  • Page 1 of 1 (3 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692