Loading ...
Home » Spaces » Smart-UPS & Symmetra LX / RM » discussion » General » INTERNAL RBC DISCONNECTED - 02000 ERROR

INTERNAL RBC DISCONNECTED - 02000 ERROR

Discussion in Smart-UPS & Symmetra LX / RM started by Mannie , 7/14/2016 11:55 AM
Login to follow, share, and participate in this space.
Not a member?Join now
  • mannie37
    Mannie
    New Member New Member
    Mannie 7/14/2016 11:55 AM

    I have this

    UPS APC UPS
    model :  SRT5KXLI
    S/N :  Q51444272468

     

    and I am receiving an alarm and mentioning the error 02000.

    I've checked the alarm status and mentioned there that the

    internal RBC is disconnected. Could you please help me.

    and maybe you can give me your support here in Jeddah, KSA.

    Thank you.

  • s.v.s
    svs
    =S= Representative
    svs 7/14/2016 12:53 PM (in response to Mannie)

    Hi Mannie,

    This alarm indicates one or both RBC modules of the internal battery pack are disconnected. You can try clearing the alarm   by disconnecting and reconnecting the two battery modules then running a self-test with at least 500W load connected. If the alarm   persists, brain dead the UPS by removing its input, then turn off the UPS Output from the display under Control menu. Pressing the On/Off button of the UPS at this stage will enable you to select Internal Power Off. If the alarm still persists, you should upgrade to the latest UPS and embedded network card firmware revisions. Local support (contact info below) will be able to assist with the guide and the necessary firmware files.

    http://www.apc.com/sa/en/support/contact-us/index.jsp

    http://www.apc.com/sa/en/support/contact/ask_apc.cfm

  • asepsehabudi72
    Asep
    New Member New Member
    Asep 5/13/2017 5:18 AM (in response to svs)

    Dear Mr.SVS,

    I have the same problem right now, i've Apc SRT10kva and first problem is "Check Battery Cable" then i've try clearing alarm by disconnecting and reconnecting battery modul then running again but not solve, and then i've try removing input and turn off UPS output then finally solved alarm.

    but for a view day UPS problem again by the same alarm, I submitted the same thing as yesterday but instead add alarm that is "check battery cableandinternalRBC disconnected", so now there are 2 and I do the same thing but it did not work. Is there a way out ?

    Can you provide steps to install firmware ups update?

    Thank you.....

  • liamg
    Liam
    =S= Representative
    Liam 5/15/2017 8:15 PM (in response to Asep)

    Hello - 

    You can find information on upgrading Firmware via the Firmware Upgrade Wizard here:

    http://www.apc.com/us/en/faqs/index?page=content&id=FA279197

    If you prefer to upgrade via the Network Management Card, that can be found here:

    http://www.apc.com/us/en/faqs/index?page=content&id=FA281753

    thanks,

    Liam

  • Page 1 of 1 (4 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692