Loading ...
Home » Spaces » Back-UPS & Surge Protectors » discussion » General » Back-UPS 700 - powers off and 5 second beeps

Back-UPS 700 - powers off and 5 second beeps

Discussion in Back-UPS & Surge Protectors started by David , 9 days ago
Login to follow, share, and participate in this space.
Not a member?Join now
  • gingerdog
    David
    New Member New Member
    David 9 days ago

    Hi,

    I have a back-ups 700, it's connected to a Debian box (output from apcaccess below).

    Last night and about a week ago, I found out it had turned itself off at about 4am, and was making a 5 second beep followed by about a 1 second pause when I arrived at my office later on.

    Pressing it's power button stopped it beeping and pressing it again caused it to turn on and operate normally.

    We've not had any power outages (microwave clock is fine afterall!) and there's nothing being written in the log files on my attached Linux box - so I feel it's probably a sudden/abrupt power down event on the attached computers.

    Any suggestions?

    thanks

    David.

    HOSTNAME : orange
    VERSION : 3.14.14 (31 May 2016) debian
    UPSNAME : orange
    CABLE : USB Cable
    DRIVER : USB UPS Driver
    UPSMODE : Stand Alone
    STARTTIME: 2018-07-10 08:48:24 +0100
    MODEL : Back-UPS XS 700U
    STATUS : ONLINE
    LINEV : 254.0 Volts
    LOADPCT : 34.0 Percent
    BCHARGE : 100.0 Percent
    TIMELEFT : 14.2 Minutes
    MBATTCHG : 5 Percent
    MINTIMEL : 3 Minutes
    MAXTIME : 0 Seconds
    SENSE : Medium
    LOTRANS : 140.0 Volts
    HITRANS : 300.0 Volts
    ALARMDEL : 30 Seconds
    BATTV : 13.8 Volts
    LASTXFER : No transfers since turnon
    NUMXFERS : 0
    TONBATT : 0 Seconds
    CUMONBATT: 0 Seconds
    XOFFBATT : N/A
    SELFTEST : NO
    STATFLAG : 0x05000008
    SERIALNO : 3B1743X03189
    BATTDATE : 2017-10-24
    NOMINV : 230 Volts
    NOMBATTV : 12.0 Volts
    NOMPOWER : 390 Watts
    FIRMWARE : 924.Z3 .I USB FW:Z3
    END APC : 2018-07-10 09:21:42 +0100

  • Page 1 of 1 (1 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692