Loading ...
Home » Spaces » Back-UPS & Surge Protectors » discussion » General » SC-1000 running standalone (no computer) for home entertainment system needs to run a self test

SC-1000 running standalone (no computer) for home entertainment system needs to run a self test

Discussion in Back-UPS & Surge Protectors started by Larry , 18 days ago
Login to follow, share, and participate in this space.
Not a member?Join now
  • e415ldc
    Larry
    New Member New Member
    Larry 18 days ago

    I have just replaced the battery in my SC-1000 with a new RBC-33 from APC. The manual states i should execute a self test to clear the replace battery alarm. But the manual doesn't say how to execute a self test. There is no computer involved, so no powerchute. I do not even have a cable to connect it to a computer since it didn't have one with it when I ordered it directly from APC via an upgrade through APC three years ago.

    Bottom line: I need to be able to reset the replace battery alarm on an SC-1000 without the use of a computer.

    Thank you for any help you can provide.

  • wpasquil
    Bill
    =S= Representative
    Bill 16 days ago (in response to Larry)

    Hi,

    The UPS performs a self-test automatically when turned on, and every two weeks thereafter (by default). If you power cycle the UPS it will run a self-test. 

  • Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692