Loading ...
Home » Spaces » Back-UPS & Surge Protectors » discussion » General » APC 900 with NUT

APC 900 with NUT

Discussion in Back-UPS & Surge Protectors started by Vinc , 14 days ago
Login to follow, share, and participate in this space.
Not a member?Join now
  • vikozo
    Vinc
    New Member New Member
    Vinc 14 days ago

    Hello
    i have a APC 900 conected with USB to a Raspberry Pi which has a NUT installation to manage. Final Goal is to do a safe shutdown of a Proxmox Server and a FreeNAS NAS.
    I do see the Input Voltage but not the output of it

    i have this from the Command
    # upsc APC900

    battery.charge: 100
    battery.charge.low: 10
    battery.charge.warning: 50
    battery.date: 2001/09/25
    battery.mfr.date: 2014/01/06
    battery.runtime: 920
    battery.runtime.low: 120
    battery.type: PbAc
    battery.voltage: 27.1
    battery.voltage.nominal: 24.0
    device.mfr: American Power Conversion
    device.model: Back-UPS RS 900G
    device.serial: 3B1402X00102
    device.type: ups
    driver.name: usbhid-ups
    driver.parameter.pollfreq: 30
    driver.parameter.pollinterval: 2
    driver.parameter.port: auto
    driver.parameter.synchronous: no
    driver.version: 2.7.4
    driver.version.data: APC HID 0.96
    driver.version.internal: 0.41
    input.sensitivity: medium
    input.transfer.high: 294
    input.transfer.low: 176
    input.voltage: 235.0
    input.voltage.nominal: 230
    ups.beeper.status: enabled
    ups.delay.shutdown: 20
    ups.firmware: 879.L4 .I
    ups.firmware.aux: L4
    ups.load: 53
    ups.mfr: American Power Conversion
    ups.mfr.date: 2014/01/06
    ups.model: Back-UPS RS 900G
    ups.productid: 0002
    ups.realpower.nominal: 540
    ups.serial: 3B1402X00102
    ups.status: OL
    ups.test.result: No test initiated
    ups.timer.reboot: 0
    ups.timer.shutdown: -1
    ups.vendorid: 051d

  • Page 1 of 1 (1 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692