Loading ...
Home » Spaces » Back-UPS & Surge Protectors » discussion » General » Question Regarding Humidity

Question Regarding Humidity

Discussion in Back-UPS & Surge Protectors started by Shaun , 3/23/2018 7:13 PM
Login to follow, share, and participate in this space.
Not a member?Join now
  • Schmooie
    Shaun
    New Member New Member
    Shaun 3/23/2018 7:13 PM

    I recently bought me and APC backUPS 450va to plug my PC into to protect me against brownouts. My concern is the humidity as I live in Louisiana - where it can get quite humid, especially during the summer months when it can get quite warm in my room. Anyhow, is this something I should be concerned about while using a UPS? Or do the benefits of using one outweigh what the humidity can cause?

  • wpasquil
    Bill
    =S= Representative
    Bill 3/26/2018 12:46 PM (in response to Shaun)

    Hi,

    If the Back-UPS is a BE450G these are the environment thresholds

    • Operating Temperature 32 - 104 °F ( 0 - 40 °C )
    • Operating Relative Humidity 5 - 95 %
    • Operating Elevation 0-10000ft ( 0-3000meters )
    • Storage Temperature -15 - 45 °C
    • Storage Relative Humidity 5 - 95 %
    • Storage Elevation 0-50000ft ( 0-15000meters )
    • Audible noise at 1 meter from surface of unit 45.0dBA
    • Online thermal dissipation 16.0BTU/hr
  • Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692