Loading ...
Home » Spaces » Back-UPS & Surge Protectors » discussion » General » BK350 everyday shut down issue

BK350 everyday shut down issue

Discussion in Back-UPS & Surge Protectors started by bobby , 11 days ago
Login to follow, share, and participate in this space.
Not a member?Join now
  • BobbyH
    bobby
    Novice Novice
    bobby 11 days ago

    HI , 

    I got a BK350 UPS, everyday it operate is fine, but when 1830- next day 8am, it will shut down automatically, and will auto turn on in next day 8AM, it is new buy UPS, no change any setting, base on default. then we check our building, the power supply is fine, and we would like to know, why the UPS will become like that. and anything i can do reset ? or use the interface button to reset it? and is it the timer include of this UPS?

    Bobby,

  • wpasquil
    Bill
    =S= Representative
    Bill 11 days ago (in response to bobby)

    Hi,

    The BK350 does not have a timer feature built in.

    What are the exact model and serial numbers? You will find them on bar code sticker located on the bottom of the UPS. 

    Example 

    Another question, do you have the USB cable attached and if so are you running any monitoring software? 

  • BobbyH
    bobby
    Novice Novice
    bobby 10 days ago (in response to Bill)

    HI bill, thanks update.

    the model is 

    BK350EI, 

    Serial number is : 4B1739P34462

  • wpasquil
    Bill
    =S= Representative
    Bill 10 days ago (in response to bobby)

    Hi,

    Do you have the USB cable attached and if so are you running any monitoring software? 

  • BobbyH
    bobby
    Novice Novice
    bobby 6 days ago (in response to Bill)

    it is running the Auto door operation system only. only control the one system to sense to open the door when the staff was tap on, and tap out.

  • Page 1 of 1 (5 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692