Loading ...
Home » Spaces » Back-UPS & Surge Protectors » discussion » General » Can 2 (just 2, no more) apc battery backups, be pluged from one to another, to extend the coverage?

Can 2 (just 2, no more) apc battery backups, be pluged from one to another, to extend the coverage?

Discussion in Back-UPS & Surge Protectors started by Mike , 2/5/2018 5:42 PM
Login to follow, share, and participate in this space.
Not a member?Join now
  • Mike-Lynch
    Mike
    New Member New Member
    Mike 2/5/2018 5:42 PM

    I have two identical units.

    I want to extend the battery protection of out POS PC in the event of an extended power outage.

    Thanks,

    Mike

  • wpasquil
    Bill
    =S= Representative
    Bill 2/6/2018 4:30 PM (in response to Mike)

    Hi,

    Plugging a UPS into another is not a supported configuration and if the UPS are Back-UPS the runtime will not increase. If you need increased runtime you should replace the Back-UPS with a UPS that you can add a external battery pack to. Smart-UPS SMX model UPS allow you to add multiple battery packs. Back-UPS BX1500M, BR1500G, BX1350M, and BX800M allow you to add a single battery pack. 

  • Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692