Loading ...
Home » Spaces » Back-UPS & Surge Protectors » discussion » General » Backup UPS CS 650 slowly discharging daily

Backup UPS CS 650 slowly discharging daily

Discussion in Back-UPS & Surge Protectors started by Tom , 1/8/2018 1:30 PM
Login to follow, share, and participate in this space.
Not a member?Join now
  • f14driver
    Tom
    Novice Novice
    Tom 1/8/2018 1:30 PM

    Hello First post here,

    In my private environment I'm using 3 different UPS'es. One of the is the CS 650, used to provide power to my router and a switch in case of power failure.

    The average load on the UPS is 5%.

    Since a few days I'm monitoring it through a raspberry PI and Domoticz ( via the apcupsd software).

    What strikes me as being odd is that the CS 650 UPS discharges slowly during the day down to 28% and then recharges again to 100%.

    This discharge is happening daily ( and decreasing the run time as well off course) and I would like to know if this behaviour is normal for this UPS type.

    The UPS has no alarms triggering or is indication there's a fault so It seems the be working fine.

    My other 2 APC UPS'es (SUA750XL & SMT750i) don't display this behaviour and remain fully loaded at 100%.

    Discharge daily

    Load voltage

    Thank you in advance for your responses

    Tom

  • f14driver
    Tom
    Novice Novice
    Tom 1/12/2018 10:20 PM (in response to Tom)

    This question can be removed.

    After monitoring closely for a few days I've come to the conclusion that the battery is faulty and/or the load voltage isn't stable. I understand that these issues are linked ( voltage opposite to battery level) so it could also be a faulty capacitor in the load unit itself.

    Rather then risking the same issue with a new battery I've decided to replace the entire unit.

    The UPS has been removed from operation and replaced by a SMT750i with an AP9630 management card :-)

    Too bad no one from APC was able to comment on the situation I had.

  • Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692