Loading ...
Home » Spaces » » »

Universal Transfer Switch

Login to follow, share, and participate in this space.
Not a member?Join now
Search
Recent Posts
Last post
ipicKedawinna
by Angela
How big of a UPS can I use for the UTS10BI?
ketchn
by Nelson
italyguy01
by Italyguy01
UTS6H L14-30 Hardwire Kit - That's It?
faktor
by Mark
What have you used as a RADIUS server?
breda1311
by Breda
UTS6H install location
elorimer
by E.
Charging a RBC7 without UPS
Llewellyn
by Llewellyn
No Error but battery has no capacity
Llewellyn
by Llewellyn
ipicKedawinna
by Angela
Galaxy 300 CLA model
ipicKedawinna
by Angela

Space Overview

Post questions regarding APC's Universal Transfer Switch here. The APC Universal Transfer Switch (UTS) monitors the utility power conditions of your home or small business and safely transfers loads to TWO backup power sources when a power disturbance occurs. Power is conveniently distributed from the backup sources to as many as ten circuits, keeping critical loads such as lights, furnaces, well pumps, and home appliances up and running during an outage. Unlike other transfer switches that are compatible only with generators, the UTS can also be connected to a UPS.

Space Administrators

Leave Space


Add a new tab

Add a hyperlink to the space navigation. You can link to internal or external web pages. Enter the Tab name and Tab URL. Upload or choose an icon. Then click Save.

Tab name The name that will appear in the space navigation.
Tab URL The url can point to an internal or external web page.
Choose your language:  
powered by Communifire
Version 5.2.6420.11692