Loading ...
Home » Spaces » » »

Universal Transfer Switch

Login to follow, share, and participate in this space.
Not a member?Join now
Search
Recent Posts
Last post
UTS6 AND EU3000I
Notes
by Andy
I have three 240V 2 pole circuits...BUT
ipicKedawinna
by Angela
UTS6H Grounding
ipicKedawinna
by Angela
ipicKedawinna
by Angela
hoangthi
by PHAM
UTS6H: How To Deal With Problem Startup Load?
hondabill
by William
How to connect a Honda EU2000i to a UTS6?
sludden88
by Shanon

Space Overview

Post questions regarding APC's Universal Transfer Switch here. The APC Universal Transfer Switch (UTS) monitors the utility power conditions of your home or small business and safely transfers loads to TWO backup power sources when a power disturbance occurs. Power is conveniently distributed from the backup sources to as many as ten circuits, keeping critical loads such as lights, furnaces, well pumps, and home appliances up and running during an outage. Unlike other transfer switches that are compatible only with generators, the UTS can also be connected to a UPS.

Space Administrators

Leave Space


Add a new tab

Add a hyperlink to the space navigation. You can link to internal or external web pages. Enter the Tab name and Tab URL. Upload or choose an icon. Then click Save.

Tab name The name that will appear in the space navigation.
Tab URL The url can point to an internal or external web page.
Choose your language:  
powered by Communifire
Version 5.2.6420.11692