Loading ...
Home » Spaces » » »

Universal Transfer Switch

Login to follow, share, and participate in this space.
Not a member?Join now
Search
Recent Posts
Last post
UnexpectedBill
by William
Using (2) UTS-10bi
dbowman89
by Daniel
UTS6BI only 4 120v circuits?
wayne_i
by Wayne
Brian309
by Brian
Regarding Circuits 5 and 6 in a UTS6H
MadJack
by Jack
UTS6H and UPS questions
peani
by Pablo
UTS10BI - Doubling up circuts
wpasquil
by Bill
UTS6H 3rd edition vs. older editions
wacodusm
by Will
How do I reset circuit breaker on 10BI?
moran
by Robert
wacodusm
by Will

Space Overview

Post questions regarding APC's Universal Transfer Switch here. The APC Universal Transfer Switch (UTS) monitors the utility power conditions of your home or small business and safely transfers loads to TWO backup power sources when a power disturbance occurs. Power is conveniently distributed from the backup sources to as many as ten circuits, keeping critical loads such as lights, furnaces, well pumps, and home appliances up and running during an outage. Unlike other transfer switches that are compatible only with generators, the UTS can also be connected to a UPS.

Space Administrators

Leave Space


Add a new tab

Add a hyperlink to the space navigation. You can link to internal or external web pages. Enter the Tab name and Tab URL. Upload or choose an icon. Then click Save.

Tab name The name that will appear in the space navigation.
Tab URL The url can point to an internal or external web page.
Choose your language:  
powered by Communifire
Version 5.2.6420.11692