Loading ...
Home » Spaces » » »

Universal Transfer Switch

Login to follow, share, and participate in this space.
Not a member?Join now
Recent Posts
Last post
UTS6H - LCD Display
by Michelle
by Jim
Slowly Exposing Circuits to my Generator
by Russ
UTS6H - load phases and neutral bond?
by Russ
Making the UTS6 work with the Honda eu2000i
by Russ
UTS10BI Remote Start
by Russ
Transfer switch info requested
by Wayne
Inrush & Load Shedding Question
by William
by William
Using (2) UTS-10bi
by Daniel

Space Overview

Post questions regarding APC's Universal Transfer Switch here. The APC Universal Transfer Switch (UTS) monitors the utility power conditions of your home or small business and safely transfers loads to TWO backup power sources when a power disturbance occurs. Power is conveniently distributed from the backup sources to as many as ten circuits, keeping critical loads such as lights, furnaces, well pumps, and home appliances up and running during an outage. Unlike other transfer switches that are compatible only with generators, the UTS can also be connected to a UPS.

Space Administrators

Leave Space

Add a new tab

Add a hyperlink to the space navigation. You can link to internal or external web pages. Enter the Tab name and Tab URL. Upload or choose an icon. Then click Save.

Tab name The name that will appear in the space navigation.
Tab URL The url can point to an internal or external web page.
Choose your language:  
powered by Communifire
Version 5.2.6420.11692