Loading ...
home » spaces » Universal Transfer Switch » discussion » General » samrt ups, surtd5000, power failed, battery life ran out, power came back.

samrt ups, surtd5000, power failed, battery life ran out, power came back.

Discussion in Universal Transfer Switch started by Austin , 6/29/2009 5:58 PM
Login  to follow, share, and participate in this space.
Not a member?Join now
  • wodimkpa
    Austin
    New Member
    New Member
    Austin 6/29/2009 5:58 PM

    Hi all,

    I am using the SURTD5000 to power some cisco switches in my network, when the main power failed, most time on weekend, the battery life run out, but when the main power come back, the ups will not power on itself, I have to mannually reset the UPS, SO WHY WILL THE UPS NOT POWER ITSELF UP?.

    Austin
    ICT Department

  • ipicKedawinna
    Angela
    =S= Representative
    Angela 6/29/2009 7:54 PM (in response to Austin)

    one thing i can think to check is to log into the network management card and navigate to the UPS->Powerchute->Configuration section of the network management card and ensure that the On-Battery Shutdown Behavior: is set to Restart when power is restored.

    also, if you can provide the data and event logs from the UPS that would be a big help too.

    [check here to see how to do that|http://nam-en.apc.com/cgi-bin/nam_en.cfg/php/enduser/std_adp.php?p_faqid=9321]

    thanks

  • Page 1 of 1 (2 items)
powered by Communifire
Version 5.0.5741.40378
Choose your language:  English