Loading ...
Home » Spaces » Universal Transfer Switch » discussion » General » BR800 fetures question (new question!)

BR800 fetures question (new question!)

Discussion in Universal Transfer Switch started by Tamzeed , 3/12/2010 9:50 AM
Login to follow, share, and participate in this space.
Not a member?Join now
  • tamzeed
    Tamzeed
    New Member New Member
    Tamzeed 3/12/2010 9:50 AM

    Hello al,

    I'm about to buy a APC BR800 tomoroow. I have a few questions before I but that UPS.

    1) I know the Powerchute software can shut down my PC during a power outage. When mains power comes back on, can the BR 800 start up my computer automatically?

    2) Is there anyway of muting the audible alarms of the BR800 using the Powerchute software?

    Thanks.

    Message was edited by: tamzeed

  • buzz
    Laurie
    =S= Representative
    Laurie 3/12/2010 8:31 PM (in response to Tamzeed)

    1) Yes, as long as you select the correct option in your computer's BIOS that tells it to turn back on once power returns (i.e. the UPS turning off & back on after utility is restored).

    2) Yes, you can configure alarm options via the PowerChute Personal Edition software.

  • tamzeed
    Tamzeed
    New Member New Member
    Tamzeed 3/13/2010 5:17 PM (in response to Laurie)

    Ive got another question regarding the BR 800

    I am planning to connect my router, modem along with my monitor and PC to the BR 800.

    When the Power Chute software shutdowns the PC during a power outtage and the router, modem and monitor are still switched on (from power from the UPS battery), will the BR 800 continue to provide power to the router, modem and monitor till it runs out? Or will it shut itself off as well after it has shutdown the PC, thus not providing power the router, modem and monitor?

  • Techie
    Bala
    =S= Representative
    Bala 3/15/2010 10:08 AM (in response to Tamzeed)

    the UPS will shut power to its battery backup outlets after the PC has shutdown gracefully by the PCPE software after the UPS has on battery for X mins.

  • Techie
    Bala
    =S= Representative
    Bala 3/15/2010 10:23 AM (in response to Tamzeed)

    the UPS will shut power to its battery backup outlets after the PC has shutdown gracefully by the PCPE software after the UPS has on battery for X mins.

  • Page 1 of 1 (5 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692