Loading ...
Login to follow, share, and participate in this space.
Not a member?Join now

Discussions

General

This is a forum for general discussions.

Discussions: 995   ·   Last Post: Re: APC Smart-ups 1500 LEDs blinking simultaneously by PHAM 6 days ago

Space Overview

Post questions regarding APC's Universal Transfer Switch here. The APC Universal Transfer Switch (UTS) monitors the utility power conditions of your home or small business and safely transfers loads to TWO backup power sources when a power disturbance occurs. Power is conveniently distributed from the backup sources to as many as ten circuits, keeping critical loads such as lights, furnaces, well pumps, and home appliances up and running during an outage. Unlike other transfer switches that are compatible only with generators, the UTS can also be connected to a UPS.

Actions

Space Administrators

Leave Space


Add a new tab

Add a hyperlink to the space navigation. You can link to internal or external web pages. Enter the Tab name and Tab URL. Upload or choose an icon. Then click Save.

Tab name The name that will appear in the space navigation.
Tab URL The url can point to an internal or external web page.
Choose your language:  
powered by Communifire
Version 5.2.6420.11692