Loading ...
Home » Spaces » General Questions & Suggestions » discussion » General » Which USV with Network Card to use ?

Which USV with Network Card to use ?

Discussion in General Questions & Suggestions started by Goetz , 8/11/2017 2:21 AM
Login to follow, share, and participate in this space.
Not a member?Join now
  • GoetzPhil
    Novice Novice
    Goetz 8/11/2017 2:21 AM

    Sorry if I post this here but APC website is too frustrating to search 

    I need a USV that can support my 2PC so it should be around 1000VA - BUT it need to have the network card as I need to signal all components when power outage appears.

    Which USV are that - like I said unfortunatley Im not the guy clicking on all the possible USV on the APC website and reading the specs just to see its not fin in 99%.
    WHY dont they tell this directly or make a check button for this feature ?

  • wpasquil
    =S= Representative
    Bill 8/14/2017 12:45 PM (in response to Goetz)


    You should look at Smart-UPS SMT or SMX models. Those models have a smart slot that a network management card can be installed in. The available network management cards are AP9630 or AP9631.

  • Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692