Loading ...
Home » Spaces » General Questions & Suggestions » discussion » General » Can someone explain what field upgradable via UART actually means?

Can someone explain what field upgradable via UART actually means?

Discussion in General Questions & Suggestions started by ada , 4/12/2017 7:31 AM
Login to follow, share, and participate in this space.
Not a member?Join now
  • Adalinn
    ada
    New Member New Member
    ada 4/12/2017 7:31 AM

    Hi  all,

     

    Can  someone  explain  what  field  upgradable  via  UART  actually  means?

     

    Am  I  limited  only  to  the  ISSC  Bluetooth  Flash  Tool  and  updating  the  module  using  the  GUI?

     

    Are  there  not  any  ISSC  flash  tools  that  are  command  line  driven  to  automate  the  firmware  upgrade  process ?

     

    I  take  it  also  there  is  no  OTA  option  for  the  module  like  the  RN4020?

     

    Thanks

  • wpasquil
    Bill
    =S= Representative
    Bill 4/12/2017 12:46 PM (in response to ada)

    Hi,

    Are you asking about a specific APC by Schneider Electric product if not this is not an appropriate topic for this forum. The RN4020 is a bluetooth micro chip and not a covered product. If the product is APC by Schneider Electric what is the model number?

  • Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692