Loading ...
Home » Spaces » General Questions & Suggestions » discussion » General » SMX1500RM2U - Power Overload warning - with nothing plugged in

SMX1500RM2U - Power Overload warning - with nothing plugged in

Discussion in General Questions & Suggestions started by kevin , 10/21/2016 10:46 AM
Login to follow, share, and participate in this space.
Not a member?Join now
  • kevinfor
    kevin
    Novice Novice
    kevin 10/21/2016 10:46 AM

    We plug in an SMX1500RM2U unit that has been in storage for a few months... it completes the self test normally.. imput/output voltage shows 115V 60hz battery 100% - there is nothing plugged into the unit 0 Load.. after about 30mins the red light on the front (triangle with ! inside) and the unit will beep once every 60 seconds with the words "Warning Power overload" 

    it is an older version of this model  (probably 5yrs old don't have firmware/ser# in front of me right now) but I remember the UPS Couldn't be firmware updated via the AP9630 only by a serial port which we didn't have any PC's with this connection..  has anyone seen this problem before?

     

  • RealTech
    Mojtaba
    Novice Novice
    Mojtaba 12/18/2016 4:28 PM (in response to kevin)

    Your ups are over heat, and maybe the big chock inside ups are shorted and after a while this error happen.

    Eng Mojtaba Sultani
  • Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692