Loading ...
home » spaces » Other Products, Topics, & Discussions » discussion » General » Advisable Maximum Percentage Load of UPS

Advisable Maximum Percentage Load of UPS

Discussion in Other Products, Topics, & Discussions started by Jervee , 1/11/2017 10:22 AM
Login  to follow, share, and participate in this space.
Not a member?Join now
  • Zephyr
    Jervee
    Novice
    Novice
    Jervee 1/11/2017 10:22 AM

    Would just like to ask if there is a document stating that the advisable maximum load that we can have for a certain UPS is up to let say 60,70, or 80%. By the way, I'm referring to Symmetra PX 2 - 48kW. Or if there is none, what is the reason why it is only advisable to have a unit to that percentage maximum only? (Aside from the lower runtime reason, or overload issues). Hoping for a positive feedback. Thank you. smile

  • Page 1 of 1 (1 items)
Choose your language:  English  
powered by Communifire
Version 5.0.5741.40378