Loading ...
home » spaces » NetBotz Hardware & Software » discussion » General » temperature value from AP9520TH EMU by SNMP

temperature value from AP9520TH EMU by SNMP

Discussion in NetBotz Hardware & Software started by Ronald , 9/13/2011 8:48 PM
Login  to follow, share, and participate in this space.
Not a member?Join now

Note: No new discussion posts are allowed in this area. Historical content is for viewing purposes only. NetBotz are actively supported at its own standalone community - http://dcimsupport.apc.com

  • ronaldJC
    New Member
    New Member
    Ronald 9/13/2011 8:48 PM

    Hi, I am monitoring the AP9520TH device with a software called Zenoss. but i cant get the value of temperature on the sensor. i need to know what kind of Oid I can use to collect the temperature value from the sensor?

    can anybody help me? please...

  • TaSpEc
    Andrew 9/15/2011 2:30 AM (in response to Ronald)

    Unfortunately the AP9520TH is not a network enabled device. It actually communicates through A-Link protocol over RJ-45. In order to monitor this sensor, you would need to have one of the following APC environmental monitoring systems: AP9320, AP9340, NBRK201, NBRK0451, NBWL0455, or NBRK0551. The AP9319 may be able to monitor this device as well. However as previously stated, it will not work by itself.

    If you have the sensor connected to one of these devices and you can get the temperature reading via the monitoring systems web interface/Advanced view. Than I would recommend downloading either the Powernet mib for APXXXX/NBRK201 or Netbotz V3 mib for the NBXXXXXX equipment.

    Hope this information helps.

  • Page 1 of 1 (2 items)
Choose your language:  English  
powered by Communifire
Version 5.0.5741.40378