Note: No new discussion posts are allowed in this area. Historical content is for viewing purposes only. NetBotz are actively supported at its own standalone community - https://help.se-dmaas.com
Hi,
I have 3 datacenters (they are all interconnected) and I want to monitor them all. Do I need to buy 3 netbotz? Or Can I have 1 primary netbotz and 2 secondary? If so, can you give me the model of the secondary one? What is the best deployment for this case?
Thanks in advance for your help.
Have a nice day
I can use netbotz appliance and NetBotz Rack Sensor Pod 150. But Can I connect them throught a switch?
NetBotz are actively supported at its own standalone community - http://dcimsupport.apc.com Please post your questions on the dcimsupport.aps.com forum.
Thank you,
Choose a location
discussion :
There are no forums in this space.