Loading ...
Home » Spaces » NetBotz Hardware & Software » discussion » General » NetBotz Rack Monitor 570 endless reset

NetBotz Rack Monitor 570 endless reset

Discussion in NetBotz Hardware & Software started by Viktor , 9/17/2017 8:23 AM
Login to follow, share, and participate in this space.
Not a member?Join now
Announcement 

Note: No new discussion posts are allowed in this area. Historical content is for viewing purposes only. NetBotz are actively supported at its own standalone community - https://help.se-dmaas.com

  • veter2005
    Viktor
    New Member New Member
    Viktor 9/17/2017 8:23 AM

    The device has stopped responding. When connected to the console, it displays:

    U-Boot 1.1.4 (Aug 27 2014 - 14:13:56)
    MPC8248 Reset Status: Software Watchdog, External Soft, External Hard
    MPC8248 Clock Configuration
     - Bus-to-Core Mult 3x, VCO Div 4, 60x Bus Freq  16-50 , Core Freq  50-150
     - dfbrg 0, corecnf 0x10, busdf 3, cpmdf 1, plldf 0, pllmf 3
     - vco_out  400000000, scc_clk  100000000, brg_clk  100000000
     - cpu_clk  300000000, cpm_clk  200000000, bus_clk  100000000
     - pci_clk   33333333
    CPU:   MPC8248 (HiP7 Rev 14, Mask 1.0 1K50M) at 300 MHz
           Watchdog enabled
    I2C:   ready
    DRAM:  128 MB
    FLASH: 64 MB


    Does not respond to keystrokes. This message is updated every 5-6 seconds. What can I do?

  • wpasquil
    Bill
    =S= Representative
    Bill 9/18/2017 6:58 PM (in response to Viktor)

    Hi,

    NetBotz are actively supported at its own standalone community - http://dcimsupport.apc.com

  • Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692