Loading ...
Home » Spaces » NetBotz Hardware & Software » discussion » General » Receiving temperature alert even though it does not exceed threshold

Receiving temperature alert even though it does not exceed threshold

Discussion in NetBotz Hardware & Software started by Ben , 5/4/2016 1:47 PM
Login to follow, share, and participate in this space.
Not a member?Join now
Announcement 

Note: No new discussion posts are allowed in this area. Historical content is for viewing purposes only. NetBotz are actively supported at its own standalone community - https://help.se-dmaas.com

  • bmcmillon
    Ben
    New Member New Member
    Ben 5/4/2016 1:47 PM

    Received the following alert:

    Alert Description:The value of 'Temperature (1)' was too low, but has now returned to normal.
    Alert Type:Value Too Low
    Severity:Error (returned to normal)
    Alert Level:Return To Normal
    Sensor:Temperature (1)
    Sensor Value:71.2 °F
    Access information:õR
    Pod:Sensor Pod
    Time Detected:05/03/2016 01:47:04 AM
    Time Returned to Normal:05/03/2016 01:47:04 AM
    Notification Time:05/03/2016 01:47:08 AM
    Threshold Name:Default
    Action Name:Primary E-mail Notification
    Alert ID:nbErrorCond_AB7A8D78
    Version:V4_5_0_20150518_1808
    Graph of 'Temperature (1) - Sensor Pod' from 05/03/2016 12:47:04 AM to 05/03/2016 01:47:08 AM - return to normal

    We did not receive an email indicating that the temperature dropped too low, just the alert saying it returned to normal.  Notice that the time detected and time returned to normal are the same time.  The graphs included in the alert agree that the temperature was steady between 70-71 degrees.

    Why is it alerting and how do I prevent these false alarms?

    Thanks.

    Ben.

    Attachments
  • ipicKedawinna
    Angela
    =S= Representative
    Angela 5/4/2016 2:37 PM (in response to Ben)

    Hi Ben,

    NetBotz appliances are supported at our DCIM community @ dcimsupport.apc.com. I suggest posting your question there to take advantage of that community's expertise.

  • Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692