Loading ...
Home » Spaces » Getting Started » discussion » General » Issues with APC BX850M connecting to PowerChute network shutdown

Issues with APC BX850M connecting to PowerChute network shutdown

Discussion in Getting Started started by Christopher , 2/4/2018 4:57 AM
Login to follow, share, and participate in this space.
Not a member?Join now
  • morinookuni
    Christopher
    New Member New Member
    Christopher 2/4/2018 4:57 AM

    I recently purchased a APC BX850M, it works great for a back up but I want it to also shutdown my server gracefully in the event of a power loss. I have been trying to connect everything using PowerChute network shutdown but can not get the APC BX850M to connect with "Network Management Card". Is it possible to have this specific device to connect to the internet, does it even have a "Network Management Card"? If this device does not, can someone suggest a APC product that will connect to a network and be able to gracefully shutdown connected devices via PowerChute Network Shutdown or other utilities? 
    Also, my server is a ESXI 6.0 server with 5 Windows VMs and 1 Alienvault VM.  I would also like to add that I am inexperienced with ups backups, this is the first ever I bought.

    Thank you in advance for all the help and patients. 

  • wpasquil
    Bill
    =S= Representative
    Bill 2/6/2018 4:03 PM (in response to Christopher)

    Hi,

    You will need a Smart-UPS SMT or SMX with a network management card to communicate with PCNS. Here is a link to the Smart-UPS product page

    http://www.apc.com/shop/us/en/categories/power/uninterruptible-power-supply-ups-/network-and-server/smart-ups/N-1h89yke

    The difference between a SMT and SMX is the SMX allow you to add external battery packs to increase runtime while on battery. The SMT does not allow for external battery packs.  

  • morinookuni
    Christopher
    New Member New Member
    Christopher 2/6/2018 5:29 PM (in response to Bill)

    Thank you so much for sending me that information. I will look into that and see if I can get a smt version and create a redundant ups system with the one I currently have.

  • Page 1 of 1 (3 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692